MITSUBISHI ELECTRIC Changes for the Better

In this case study...

  • Fully automated handling, cutting and stacking of reinforcing steel meshes with sub-millimetre accuracy,
  • Advanced 3D vision technology identifies optimal pick-up points despite irregular mesh positioning,
  • Precise synchronisation of 22 drives ensures smooth and reliable material handling,
  • Integrated control, motion, safety and vision systems simplify automation architecture,
  • A 40-metre-long production system can be operated efficiently by a single person.

The construction industry needs many hard-working hands. After all, manual labor is still standard in many areas. Terhoeven GmbH & Co. KG has now tackled a typical example - the monotonous and laborious cutting of reinforcing steel mesh. The medium-sized mechanical engineering company relies on drive and automation technology from Mitsubishi Electric. The result is an innovative system that does not yet exist on the market.

The challenge: separating and lifting the mats is complex

ASA (automatic cutting system) is the name of the newly developed machine that handles, cuts and stacks the reinforcing steel meshes fully automatically. Lifting the top mat from the stack is a major challenge, as the manufacturing tolerances of the structural steel mats are in the centimeter range, but handling requires an accuracy of less than one millimeter. In addition, the individual mats do not lie neatly in the stack. For this reason, 3D image processing is used to identify six suitable pick-up points. When the grippers lift the mat, the next challenge arises: the mat bends. Three separate drives are therefore required for each of the six points in order to be able to move the grippers in all three spatial directions. During operation, the drives must be controlled precisely and synchronously.

The solution: drive and automation technology from a single source

To compensate for the deformation of the mats during lifting, 18 drives are required for the lifting gear, plus four drives for transporting the mats within the system. Servo drives from Mitsubishi Electric with the corresponding servo amplifiers are used here. The motors from the MR-J5 series are very compact and offer high dynamics. The appropriate servo drives can be coupled via intermediate circuits, which contributes to the high energy efficiency of the system. With the motion controller, the required synchronization of the drives can be optimally implemented. All other automation technology components also come from Mitsubishi Electric. FR-E800 frequency inverters are used for simple conveying tasks. And a safety PLC from the MELSEC iQ-R series controls all the processes in the system. This is supplemented by three C controllers on which the image processing runs. The protocol used is CC Link IE TSN, which enables real-time capability as well as the necessary safety-related communication. With the gigabit bandwidth offered by the open CC-Link IE TSN standard, communication between the controller, motion control and safety can be easily integrated into a network.

The result: huge system can be operated by one person

After a development period of almost two years, the first six-metre-high and over 40-metre-long ASA was put into operation in spring 2024. It is operated via a GOT control unit from Mitsubishi Electric. In addition to the touchscreen, a number of buttons and switches are also integrated to facilitate operation with gloves. Converting the system, for example to a new mat size, is very easy with the GOT control unit. Only a few tasks need to be carried out manually during set-up. In routine operation, the system can then be operated by one person.

Why it matters?

By combining motion control, safety, machine vision and networking technologies within a single automation architecture, the solution enabled reliable handling of reinforcing steel meshes despite significant dimensional variations and material deformation. The precise synchronisation of 22 servo axes, real-time communication via CC-Link IE TSN and integrated 3D image processing transformed a complex and labour-intensive process into a highly automated operation. As a result, the system delivers greater handling accuracy, improved energy efficiency and simplified operation, allowing a large-scale production system to be managed by a single operator while maintaining consistent process performance and flexibility for different mesh sizes.

Discover the solutions behind this case study

Have we sparked your interest? Contact us

0/255
Pole označená * jsou povinná.

Our Stories

2026-07-07

NEWBMS-Driven energy and facility performance

Mitsubishi Electric Automotive Czech

EN
Sledujte video na YouTube
#Automotive#Mitsubishi Electric Iconics Digital Solutions#GENESIS64#MELSEC iQ-R Series

2025-09-01

Transforming energy management with real‑time insights

Paul Rauschert Steinbach GmbH

ENDE
#Manufacturing#Energy#Sustainability#GENESIS64